SAFE.ID

Description

Returns the SafeID of the device. The SafeID returned is 0, if there are no SafeID available.

SAFE.ID is accessible through telnet.

Code

--> SAFE.ID
0x31

Context

For information on validation and CRC refer to Validation.

Related safety parameters:

Versions

Action

Version

Notes

Implemented

02-00-00-000

Implemented in SMM revision v0.32

General Information

Type

Read Only

Units

N/A

Range

All
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
SAFE.ID

37c2h

00h

Unsigned8

-

-

Read only

No